FRDM-IMX93 Yocto imx-image-core questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-IMX93 Yocto imx-image-core questions

638件の閲覧回数
Bugger
Contributor III


Build the imx-image-core for the FRDM-IMX93 board, per UG10164 this was stated as the image for Wayland.  The output in the deploy/images/imx93frdm  show this

rw-r--r-- 2 build build    1099 May 16 06:52 CRT.crt
-rw-r--r-- 2 build build     813 May 16 06:52 CRT.esl
-rw-r--r-- 2 build build    1704 May 16 06:52 CRT.key
-rw-r--r-- 2 build build   44161 May 16 06:52 bl31-imx93.bin
-rw-r--r-- 2 build build   48449 May 16 06:52 bl31-imx93.bin-optee
drwxr-xr-x 2 build build    4096 May 16 06:52 imx-boot-tools
-rw-r--r-- 2 build build    1660 May 16 06:52 lpddr4_dmem_1d_v202201.bin
-rw-r--r-- 2 build build    1408 May 16 06:52 lpddr4_dmem_2d_v202201.bin
-rw-r--r-- 2 build build   32428 May 16 06:52 lpddr4_imem_1d_v202201.bin
-rw-r--r-- 2 build build   25668 May 16 06:52 lpddr4_imem_2d_v202201.bin
-rw-r--r-- 2 build build  105792 May 16 06:52 mx93a1-ahab-container.img
drwxr-xr-x 3 build build    4096 May 16 06:52 optee
lrwxrwxrwx 2 build build      21 May 16 06:52 tee.bin -> optee/tee.mx93evk.bin
lrwxrwxrwx 2 build build      46 May 16 06:52 u-boot-imx-initial-env-imx93frdm-sd -> u-boot-imx-initial-env-imx93frdm-sd-2024.04-r0
-rw-r--r-- 2 build build    6948 May 16 06:52 u-boot-imx-initial-env-imx93frdm-sd-2024.04-r0
lrwxrwxrwx 2 build build      46 May 16 06:52 u-boot-imx-initial-env-sd -> u-boot-imx-initial-env-imx93frdm-sd-2024.04-r0
lrwxrwxrwx 2 build build      24 May 16 06:52 u-boot-imx93frdm.bin -> u-boot-sd-2024.04-r0.bin
lrwxrwxrwx 2 build build      24 May 16 06:52 u-boot-imx93frdm.bin-sd -> u-boot-sd-2024.04-r0.bin
-rw-r--r-- 2 build build 1155568 May 16 06:52 u-boot-sd-2024.04-r0.bin
lrwxrwxrwx 2 build build      28 May 16 06:52 u-boot-spl.bin -> u-boot-spl.bin-sd-2024.04-r0
lrwxrwxrwx 2 build build      28 May 16 06:52 u-boot-spl.bin-imx93frdm -> u-boot-spl.bin-sd-2024.04-r0
lrwxrwxrwx 2 build build      28 May 16 06:52 u-boot-spl.bin-imx93frdm-sd -> u-boot-spl.bin-sd-2024.04-r0
lrwxrwxrwx 2 build build      28 May 16 06:52 u-boot-spl.bin-sd -> u-boot-spl.bin-sd-2024.04-r0
-rw-r--r-- 2 build build  138854 May 16 06:52 u-boot-spl.bin-sd-2024.04-r0
lrwxrwxrwx 2 build build      24 May 16 06:52 u-boot.bin -> u-boot-sd-2024.04-r0.bin
lrwxrwxrwx 2 build build      24 May 16 06:52 u-boot.bin-sd -> u-boot-sd-2024.04-r0.bin

There aren't any rootfs not partition images files

How to go from here is build an complete image for SD or EMMC ?

 

0 件の賞賛
返信
2 返答(返信)

451件の閲覧回数
Bugger
Contributor III

Thanks, What I want was just the image or rootfs only. is it possible to extract the seperate images from the wic file ?

0 件の賞賛
返信

593件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Each image build creates a U-Boot, a kernel, and an image type based on the IMAGE_FSTYPES defined in the machine configuration file. Most machine configurations provide an SD card image (.wic) and a rootfs image (.tar). The SD card image contains a partitioned image (with U-Boot, kernel, rootfs, etc.) suitable for booting the corresponding hardware.

An SD card image file .wic contains a partitioned image (with U-Boot, kernel, rootfs, etc.) suitable for booting the corresponding hardware. To flash an SD card image, run the following command:

zstdcat <image_name>.wic.zst | sudo dd of=/dev/sd<partition> bs=1M conv=fsync

For more information on flashing, see Section "Preparing an SD/MMC card to boot" in the i.MX Linux User's Guide (UG10163)

Regards

0 件の賞賛
返信