i.MX8mp: LVDS signal adjustment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8mp: LVDS signal adjustment

Jump to solution
4,246 Views
hiroakiosawa
Contributor III

Hi.

I've been designing  i.mx8m plus board that using LVDS. Now I try to fix the  EMI matters on lvds signal to adjust the lvds signal strength with using "CC_ADJ" bits on LVDS_CTRL Register. (Naturally, lvds's tx/rx impedance is already matched at 100Ω.)

Some LVDS_CTRL Register bit description has not present specific values on i.MX8M Plus Reference Manual (screenshot attatched). Does NXP has any information for those registers ?

0 Kudos
Reply
1 Solution
4,235 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hiroaki

 

additional description was sent you via mail.

 

Best regards
igor

View solution in original post

5 Replies
527 Views
rajeevsv
Contributor III

Hi NXP team,

Could you please send the additional description to me as well. Need to tweak that LVDS_CTRL register,

Thanks in advance,
Rajeev

0 Kudos
Reply
4,236 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hiroaki

 

additional description was sent you via mail.

 

Best regards
igor

2,568 Views
agunel
Contributor I
Hi NXP team,

I also need this information. We use imx8qm with a touchscreen on LVDS1_CH0. Is it possible to change drive strength from device tree. We are using Yocto with 5.15 kernel.
0 Kudos
Reply
3,726 Views
yogeshbsa89
Contributor II

Hi Igor,

I also need this information .

could you please share this information with me.

Regards,

Yogesh

 

Tags (1)
0 Kudos
Reply
3,821 Views
Marcel_ArrowCE
Contributor II

HI NXP Team, 

 

I need also this information. 

 

Can you also share with me? 

 

BR

Marcel 

0 Kudos
Reply