I recently purchased an FRDM iMX93 development board. I followed the instructions at https://www.nxp.com/document/guide/getting-started-with-frdm-imx93:GS-FRDM-IMX93?_gl=1*zkk08q*_ga* MTUyMTQ0MDk5NS4xNzgwNTY1MTg4*_ga_WM5LE0KMSH*czE3ODA2Mzk2ODgkbzQkZzEkdDE3ODA2NDAzMDgkajQwJGwwJGg1MzYwMjA4MTc.§ion=build-and-run
When following the tutorial and running the command “$ bitbake imx-image-full”, the following error appears. How can I resolve this?
Thank you!
ERROR: linux-imx-headers-6.6-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/998/bus"; export PATH="/home/yejx/imx93/frdm-imx93/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/yejx/imx93/sources/poky/scripts:/home/yejx/imx93/frdm-imx93/tmp/work/armv8a-mx93-poky-linux/linux-imx-headers/6.6/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/yejx/imx93/frdm-imx93/tmp/work/armv8a-mx93-poky-linux/linux-imx-headers/6.6/recipe-sysroot/usr/bin/crossscripts:/home/yejx/imx93/frdm-imx93/tmp/work/armv8a-mx93-poky-linux/linux-imx-headers/6.6/recipe-sysroot-native/usr/sbin:/home/yejx/imx93/frdm-imx93/tmp/work/armv8a-mx93-poky-linux/linux-imx-headers/6.6/recipe-sysroot-native/usr/bin:/home/yejx/imx93/frdm-imx93/tmp/work/armv8a-mx93-poky-linux/linux-imx-headers/6.6/recipe-sysroot-native/sbin:/home/yejx/imx93/frdm-imx93/tmp/work/armv8a-mx93-poky-linux/linux-imx-headers/6.6/recipe-sysroot-native/bin:/home/yejx/imx93/sources/poky/bitbake/bin:/home/yejx/imx93/frdm-imx93/tmp/hosttools"; export HOME="/home/yejx"; LANG=C git -c gc.autoDetach=false -c core.pager=cat -c safe.bareRepository=all clone --bare --mirror https://github.com/nxp-imx/linux-imx.git /home/yejx/imx93/downloads//git2/github.com.nxp-imx.linux-imx.git --progress failed with exit code 128, see logfile for output
ERROR: linux-imx-headers-6.6-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/nxp-imx/linux-imx.git;protocol=https;branch=lf-6.6.y')
ERROR: Logfile of failure stored in: /home/yejx/imx93/frdm-imx93/tmp/work/armv8a-mx93-poky-linux/linux-imx-headers/6.6/temp/log.do_fetch.2202373
ERROR: Task (/home/yejx/imx93/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx-headers_6.6.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3099 tasks of which 1313 didn't need to be rerun and 9 failed.
Summary: 9 tasks failed:
/home/yejx/imx93/sources/meta-imx/meta-imx-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.24.0.imx.bb:do_fetch
/home/yejx/imx93/sources/meta-imx/meta-imx-ml/recipes-nnstreamer/nnstreamer/nnstreamer_2.2.0.bb:do_fetch
virtual:native:/home/yejx/imx93/sources/meta-imx/meta-imx-ml/recipes-libraries/tensorflow-lite/tensorflow-lite-host-tools_2.16.2.bb:do_fetch
/home/yejx/imx93/sources/meta-imx/meta-imx-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.24.0.imx.bb:do_fetch
/home/yejx/imx93/sources/meta-freescale-distro/recipes-graphics/imx-gpu-sdk/libxdg-shell.bb:do_fetch
/home/yejx/imx93/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_fetch
/home/yejx/imx93/sources/meta-imx/meta-imx-bsp/recipes-bsp/imx-atf/imx-atf_2.10.bb:do_fetch
/home/yejx/imx93/sources/meta-imx/meta-imx-bsp/recipes-bsp/imx-secure-enclave/imx-secure-enclave_git.bb:do_fetch
/home/yejx/imx93/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx-headers_6.6.bb:do_fetch
Summary: There were 30 WARNING messages.
Summary: There were 18 ERROR messages, returning a non-zero exit code.