FEC driver bug explanation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FEC driver bug explanation

1,897件の閲覧回数
vladimirovseych
Contributor III

Hello, dear Freescale!

 

Can you explain a bug with system failure under high network load?

 

I'm using i.MX287 with two ethernet controllers connected with bridge

On kernel 3.18 (OpenWRT) I catched NETDEV WATCHDOG warning and kernel oops while iperf testing (log.txt).

But when I backported your driver from 4.4.7 to 3.18.29, bug disappeared.

3 files was changed:

  • fec_main.c
  • fec.h
  • fec_ptp.c

 

What/where is the reason of the failure?

Thanks in advance.

Vladimir.

Original Attachment has been moved to: fec_ptp_old.c.zip

Original Attachment has been moved to: log.txt.zip

Original Attachment has been moved to: fec_old.h.zip

Original Attachment has been moved to: fec.h.zip

Original Attachment has been moved to: fec_main.c.zip

Original Attachment has been moved to: fec_main_old.c.zip

Original Attachment has been moved to: fec_ptp.c.zip

ラベル(3)
タグ(5)
0 件の賞賛
返信
1 返信

1,581件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vladimir

suggest to post that on linux mail list since nxp does not officially

support i.MX28 for 4.4.7 or 3.18.29 kernels. Supported bsps are located

on official web product page

i.MX28 Evaluation Kit|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信