SD Card booting is happening with any boot configuration changes compared to SPI for IMX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD Card booting is happening with any boot configuration changes compared to SPI for IMX6SL

765 Views
matrimanish
Contributor I

I am booting IMX6SL processor through SPI NOR FLASH( by default). There is another option on my board to boot via SD card. when i am trying to boot from SD card , board get booted, with any boot configuration changes. It should be booted after required boot pin configuration changes for SD card, but it is booted with same configuration which is used for SPI NOR. If SPI and SD boath are available for boot, then it get booted using SD card.It is ok with hardware pin high low configuration. Please provide any solution.

Labels (4)
0 Kudos
Reply
1 Reply

692 Views
igorpadykov
NXP Employee
NXP Employee

Hi MATRI

similar behaviour could be observed in manufacturing mode,

please check sect.8.11 SD/MMC Manufacture Mode i.MX6SL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SLRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply