FEC driver bug explanation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FEC driver bug explanation

1,383 次查看
vladimirovseych
Contributor III

Hello, dear Freescale!

 

Can you explain a bug with system failure under high network load?

 

I'm using i.MX287 with two ethernet controllers connected with bridge

On kernel 3.18 (OpenWRT) I catched NETDEV WATCHDOG warning and kernel oops while iperf testing (log.txt).

But when I backported your driver from 4.4.7 to 3.18.29, bug disappeared.

3 files was changed:

  • fec_main.c
  • fec.h
  • fec_ptp.c

 

What/where is the reason of the failure?

Thanks in advance.

Vladimir.

Original Attachment has been moved to: fec_ptp_old.c.zip

Original Attachment has been moved to: log.txt.zip

Original Attachment has been moved to: fec_old.h.zip

Original Attachment has been moved to: fec.h.zip

Original Attachment has been moved to: fec_main.c.zip

Original Attachment has been moved to: fec_main_old.c.zip

Original Attachment has been moved to: fec_ptp.c.zip

标签 (3)
0 项奖励
回复
1 回复

1,067 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vladimir

suggest to post that on linux mail list since nxp does not officially

support i.MX28 for 4.4.7 or 3.18.29 kernels. Supported bsps are located

on official web product page

i.MX28 Evaluation Kit|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复