Executing Program from SDRAM performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Executing Program from SDRAM performance

1,079件の閲覧回数
rnicolls
Contributor IV

Hi,

We'd like to copy our application from NOR flash and execute from the external SDRAM. My understanding is that the SDRAM controller is connected to a 32 bit bus, whereas the Serial NOR Flash is connected to a 64 bit bus. The result is reduced performance when executing instructions from the SDRAM. How poor will the performance be? We're using the IMXRT1176.

Thanks

0 件の賞賛
返信
1 返信

1,041件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

Yes, it is expected some reduced performance between SDRAM and Nor flash however this difference is not significant if you place text on SDRAM and data on DTCM.
I will attach an example of theoretical throughput on different RT11xx interfaces:

Omar_Anguiano_0-1671662686746.pngOmar_Anguiano_0-1671662686746.png

Best regards,
Omar

0 件の賞賛
返信