Executing Program from SDRAM performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Executing Program from SDRAM performance

1,076 Views
rnicolls
Contributor IV

Hi,

We'd like to copy our application from NOR flash and execute from the external SDRAM. My understanding is that the SDRAM controller is connected to a 32 bit bus, whereas the Serial NOR Flash is connected to a 64 bit bus. The result is reduced performance when executing instructions from the SDRAM. How poor will the performance be? We're using the IMXRT1176.

Thanks

0 Kudos
Reply
1 Reply

1,038 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

Yes, it is expected some reduced performance between SDRAM and Nor flash however this difference is not significant if you place text on SDRAM and data on DTCM.
I will attach an example of theoretical throughput on different RT11xx interfaces:

Omar_Anguiano_0-1671662686746.pngOmar_Anguiano_0-1671662686746.png

Best regards,
Omar

0 Kudos
Reply