Example of imx8mq device tree for imx219 camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example of imx8mq device tree for imx219 camera

1,602 Views
vanpye00
Contributor II

I'm trying to get the imx219 works with the imx8mq via the csi bridge but it's currently not working. Is there an example of the imx8mq device tree configuration for the imx219 ? Thanks

0 Kudos
Reply
3 Replies

1,586 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @vanpye00,

I hope you are doing well.

->This device tree configuration must include an I2C node with its clock and voltage regulator settings, and an IMX219 camera node with its clock settings, voltage regulator settings, and endpoint configuration. It must also include an OV5640 CSI node with its clock settings and endpoint configuration.

->All the ports, clock, voltage-related properties, and how to set them all these details regarding imx219 one can find at below given location.
<src_code>/Documentation/devicetree/bindings/display/tegra/nvidia,tegra20-host1x.txt

Thanks & Regards.
Dhruvit Vasavada

0 Kudos
Reply

1,572 Views
vanpye00
Contributor II
Dhruvit,

You mentioned OV5640 CSI node. Do you mean imx 219 csi node?
0 Kudos
Reply

1,560 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @vanpye00,

I hope you are doing well.

Yes, It is an imx219_a_out node, one should define it for the same.

Thanks & Regards.
Dhruvit Vasavada

0 Kudos
Reply