Ethernet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet

3,388 次查看
JaysonJacobThom
Contributor I

Hi

 

Does anyone know how to connect to the internet via Ethernet?

 

Hardware: iMX53 QSB

Software: Kernel ver: 2.6.35.3

               Android ver: 2.3.3

 

I've tried typing netcfg into the serial console & get the following ouput (only relevant part shown):

 

lo         UP    127.0.0.1       255.0.0.0       0x00000049
eth0     UP    10.150.224.243  255.255.0.0     0x00001043

When I open a browser & try to access a website, I get the error: Web page not available.

 

I've enabled Settings->Wireless & networks ->Ethernet - & it shows that its connected.

Does anyone know how to fix this problem...

 

Many thanks

Jayson

标签 (1)
0 项奖励
回复
5 回复数

3,228 次查看
EricNelson
Senior Contributor II
Glad to hear it
0 项奖励
回复

3,228 次查看
JaysonJacobThom
Contributor I

Hey Eric,

Thanks, i got it working.

 

I looked for the right DNS server IP address using 'getprop' :)

 

Jayson

0 项奖励
回复

3,228 次查看
EricNelson
Senior Contributor II

Hi Jayson,

 

Do you know what your DNS server address(es) should be? My example was just a guess.

 

I also thought 'getprop net.eth0' would show you all of the net.eth0.x variables,

but apparently not. If you run 'getprop' by itself, you can scan the list, or you can

use an ADB connection to allow you to grep on your development machine:

 

     adb shell getprop | grep net.eth0

 

Regards,

 

Eric

0 项奖励
回复

3,228 次查看
JaysonJacobThom
Contributor I

Hey Eric,

Thanks for your reply.

I still couldn't get it to work - here's the output:

/************************************************/

# getprop net.eth0.dns1

# getprop net.eth0

# netcfg
lo       UP    127.0.0.1       255.0.0.0       0x00000049
eth0     UP    10.150.224.235  255.255.0.0     0x00001043
usb0     DOWN  0.0.0.0         0.0.0.0         0x00001002
tunl0    DOWN  0.0.0.0         0.0.0.0         0x00000080
gre0     DOWN  0.0.0.0         0.0.0.0         0x00000080
sit0     DOWN  0.0.0.0         0.0.0.0         0x00000080
# setprop net.dns1 10.150.224.1
# getprop net.eth0.dns1

# gepro
gepro: not found
# getprop net.eth0

# setprop net.eth0.dns1 10.150.224.1
# getprop net.eth0.dns1
10.150.224.1
# getprop net.dns1
10.150.224.1

/************************************************/

 

Have I made any mistakes?

Thanks,

Jayson

0 项奖励
回复

3,228 次查看
EricNelson
Senior Contributor II

Hi Jason,

 

Try 'setprop net.dns1 10.150.224.1' to configure your Domain Name Server.

 

Take a look at the output of 'getprop net.eth0' for the appropriate value.

 

At least in R10.1, the scripts in /etc/dhcpcd/dhcpcd-hooks were setting the

property net.eth0.dns1-4 instead of net.dns1-4.

 

Eric

0 项奖励
回复