Hi,
We have designed a custom board with I.MX6 SoloX (MCIMX6X3EVO10AB). The whole board is very close to the eval board 6SX SABRE SDB (see relevant schematic_eth.png in attachment). The difference on our board is that only 100Mbps signals are used from RJ45 and 1Gbps Signals are not connected.
Linux of Yocto Rocko is running on it.
If the board is connected over ethernet the LED_ACT LED starts blinking. After about 15 seconds the LED_10_100 turns on and following messages are printed over serial console
fec 2188000.ethernet eth0: Link is Up - 10Mbps/Full - flow control off IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
When ethernet cable is unplugged, following messages appear:
fec 2188000.ethernet eth0: Link is Down IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
Following activity are measured on the pins:
ENET1_MDC (2.36MHz, 0..3.3V),
ENET1_MDIO (0.3..3V),
ENET2_RX_CLK (25MHz, 0..3.3V),
ENET2_TX_CLK (3 V),
ENET2_COL(0V)
ENET2_CRS (3.3V)
RGMIII1_TD[0:2] (0..1.5V, some data every few seconds )
RGMIII1_TD[3] (0..1.5V, some data bit more frequent than RGMIII1_TD[0:2] )
RGMIII1_TX_CTL (0..1.5V, some data every few seconds )
RGMIII1_TXC (2.5MHz, 0..1.5V)
RGMIII1_RD[0:3] (0..1.5V),
RGMIII1_RXC (25 MHz, 0...1.5V),
RGMIII1_RX_CTL (0..1.5V),
Suspicious things:
- TD seems to be on lower frequency than RX. This could be due to that the imx6 thinks it's 10Mbps and the PHY is on 100Mbps.
In the DeviceTree (see imx6sx-sdb.dtsi in attachment) there are following entries:
&iomuxc {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_hog &pinctrl_can_gpios>;
imx6x-sdb {
...
pinctrl_enet1: enet1grp {
fsl,pins = <
MX6SX_PAD_ENET1_MDIO__ENET1_MDIO 0xa0b1
MX6SX_PAD_ENET1_MDC__ENET1_MDC 0xa0b1
MX6SX_PAD_RGMII1_TXC__ENET1_RGMII_TXC 0xa0b1
MX6SX_PAD_RGMII1_TD0__ENET1_TX_DATA_0 0xa0b1
MX6SX_PAD_RGMII1_TD1__ENET1_TX_DATA_1 0xa0b1
MX6SX_PAD_RGMII1_TD2__ENET1_TX_DATA_2 0xa0b1
MX6SX_PAD_RGMII1_TD3__ENET1_TX_DATA_3 0xa0b1
MX6SX_PAD_RGMII1_TX_CTL__ENET1_TX_EN 0xa0b1
MX6SX_PAD_RGMII1_RXC__ENET1_RX_CLK 0x3081
MX6SX_PAD_RGMII1_RD0__ENET1_RX_DATA_0 0x3081
MX6SX_PAD_RGMII1_RD1__ENET1_RX_DATA_1 0x3081
MX6SX_PAD_RGMII1_RD2__ENET1_RX_DATA_2 0x3081
MX6SX_PAD_RGMII1_RD3__ENET1_RX_DATA_3 0x3081
MX6SX_PAD_RGMII1_RX_CTL__ENET1_RX_EN 0x3081
MX6SX_PAD_ENET2_RX_CLK__ENET2_REF_CLK_25M 0x91
>;
};
pinctrl_enet_3v3: enet3v3grp {
fsl,pins = <
MX6SX_PAD_ENET2_COL__GPIO2_IO_6 0x000010B0
MX6SX_PAD_ENET2_CRS__GPIO2_IO_7 0x000010B0
MX6SX_PAD_ENET2_TX_CLK__GPIO2_IO_9 0x000010B0
>;
};
/*
pinctrl_enet2: enet2grp {
...
};
*/
...
&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet1>;
phy-supply = <®_enet_3v3>;
phy-mode = "rgmii";
phy-handle = <ðphy1>;
status = "okay";
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy1: ethernet-phy@1 {
reg = <1>;
};
/*
ethphy2: ethernet-phy@2 {
reg = <2>;
};*/
};
};Do you have any clue where to check next what to do?
Many thanks in advance for any tips.
Regards Dani
Solved! Go to Solution.
A primary mistake here was that the pull-up to ENET_3V3 from MDIO line was missing. So the Linux OS detects the controller and can retrieve and IP and autonegotiate speed.
Now I'm experiencing following issues:
U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1b (Sep 13 2018 - 16:28:25 +0200) CPU: Freescale i.MX6SX rev1.2 996 MHz (running at 792 MHz) CPU: Extended Commercial temperature grade (-20C to 105C) at 46C Reset cause: POR Model: Freescale i.MX6 SoloX SDB RevB Board Board: MX6SX SABRE SDB DRAM: 512 MiB PMIC: PFUZE100! DEV_ID=0x11 REV_ID=0x21 MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2 *** Warning - bad CRC, using default environment Display: Hannstar-XGA (1024x768) Video: 1024x768x18 In: serial Out: serial Err: serial switch to partitions #0, OK mmc1 is current device Net: Error: ethernet@02188000 address not set. No ethernet found.
=> mii device MII devices:
fec 2188000.ethernet eth0: Link is Down IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
A primary mistake here was that the pull-up to ENET_3V3 from MDIO line was missing. So the Linux OS detects the controller and can retrieve and IP and autonegotiate speed.
Now I'm experiencing following issues:
U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1b (Sep 13 2018 - 16:28:25 +0200) CPU: Freescale i.MX6SX rev1.2 996 MHz (running at 792 MHz) CPU: Extended Commercial temperature grade (-20C to 105C) at 46C Reset cause: POR Model: Freescale i.MX6 SoloX SDB RevB Board Board: MX6SX SABRE SDB DRAM: 512 MiB PMIC: PFUZE100! DEV_ID=0x11 REV_ID=0x21 MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2 *** Warning - bad CRC, using default environment Display: Hannstar-XGA (1024x768) Video: 1024x768x18 In: serial Out: serial Err: serial switch to partitions #0, OK mmc1 is current device Net: Error: ethernet@02188000 address not set. No ethernet found.
=> mii device MII devices:
fec 2188000.ethernet eth0: Link is Down IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
The evaluation board had the same issue. After changing the switch this problem has gone.
igorpadykov: thank you for your effort.
one can try to debug it checking signals with oscilloscope in
uboot/drivers/net/fec_mxc.c, ..freescale/mx6sxsabresd/mx6sxsabresd.c
Best regards
igor
Hi igor,
Many thanks for your reply.
To try to get it work on u-boot is a great idea indeed and I will definitely try to do that. Thank you for showing me where.
According to your advice I have changed the device tree. I set rmii in the device tree by replacing the rgmii. Checking dmesg I can see:
fec 2188000.ethernet eth0: registered PHC device 0 Generic PHY 2188000.ethernet-1:01: attached PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet-1:01, irq=-1)
The messages on plugging in and out
fec 2188000.ethernet eth0: Link is Up - 10Mbps/Full - flow control off IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready fec 2188000.ethernet eth0: Graceful transmit stop did not complete! fec 2188000.ethernet eth0: Link is Down IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
With rgmii I get these messages on startup:
fec 2188000.ethernet eth0: registered PHC device 0 Generic PHY 2188000.ethernet-1:01: attached PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet-1:01, irq=-1)
And when plug and unplugging
fec 2188000.ethernet eth0: Link is Up - 10Mbps/Full - flow control off IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready fec 2188000.ethernet eth0: Link is Down IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
If I check iMX Linux Reference Manual (IMXLXRM) Table 43.1 Pin Usage in MII, RMII, p. 300, I can see that with the wiring I am using and that is used on the eval board 6SX Sabre SDB (Schematics) I should use RGMII: i.e. the signal FEC_TX_CLK is wired (used in RGMII, not in RMII) and the Transceiver (same on both boards) does only support RGMII and not RMII. With this in mind I am more convinced that the way it has been on the device tree by using RGMII must be correct. What makes you thinking differently?
Thank you again,
Dani
Hi Dani
on below case rmii in the device tree worked fine with i.MX6DL
How do I set the ENET_REF_CLK rate
Best regards
igor
Hi stimpy
first one can try to make it work in uboot, please check ethernet clocks in
setup_fec() in uboot/board/freescale/mx6sxsabresd/mx6sxsabresd.c
mx6sxsabresd.c\mx6sxsabresd\freescale\board - uboot-imx - i.MX U-Boot
"CONFIG_FEC_ENET_DEV" in uboot/include/configs/mx6sxsabresd.h
Register settings in IOMUXC_GPR_GPR1, ENET2_TX_CLK_DIR,ENET2_CLK_SEL
sect.35.4.2 GPR1 General Purpose Register (IOMUXC_GPR_GPR1) i.MX6SX Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6SXRM.pdf
In device tree one can try with
phy-mode = "rmii";
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------