Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)

Jump to solution
1,754 Views
Samhitha_Kashyap
Contributor III

Does NXP provide the Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)?

The variscite board var-som-mx8mp board has both the ethernets made available for the Cortex A-53 ( OS: Linux), I need to use one of the ethernet for Cortex M-7 ( OS: FreeRTOS).

Can anyone help me find the driver for the same.

 

0 Kudos
Reply
1 Solution
1,734 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

The Cortex-M Core are mainly intended for real-time application, delegating the high-speed communications (like ethernet and USB) to the Cortex-A cores.

With the above into account we do not provide an ethernet driver for the Cortex M7.

Best regards,
Aldo.

View solution in original post

0 Kudos
Reply
1 Reply
1,735 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

The Cortex-M Core are mainly intended for real-time application, delegating the high-speed communications (like ethernet and USB) to the Cortex-A cores.

With the above into account we do not provide an ethernet driver for the Cortex M7.

Best regards,
Aldo.

0 Kudos
Reply