Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)

跳至解决方案
1,746 次查看
Samhitha_Kashyap
Contributor III

Does NXP provide the Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)?

The variscite board var-som-mx8mp board has both the ethernets made available for the Cortex A-53 ( OS: Linux), I need to use one of the ethernet for Cortex M-7 ( OS: FreeRTOS).

Can anyone help me find the driver for the same.

 

0 项奖励
回复
1 解答
1,726 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

The Cortex-M Core are mainly intended for real-time application, delegating the high-speed communications (like ethernet and USB) to the Cortex-A cores.

With the above into account we do not provide an ethernet driver for the Cortex M7.

Best regards,
Aldo.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,727 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

The Cortex-M Core are mainly intended for real-time application, delegating the high-speed communications (like ethernet and USB) to the Cortex-A cores.

With the above into account we do not provide an ethernet driver for the Cortex M7.

Best regards,
Aldo.

0 项奖励
回复