Error when building System Control Firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error when building System Control Firmware

1,403 Views
anjalikkrishna
Contributor III

Hi,

   I am trying to build the scfw source code with few changes related to resource allocation . I have followed the below link

System Controller Firmware 101 - Resource management service 

and issued

the below command

 ./$(MKIMG) -soc QX -rev B0 -append ahab-container.img -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a35 0x80000000  -p3  -m4 m40_tcm.bin 0 0x34FE0000 -out flash.bin

But I am getting the error as unrecognized option -p3

Any help would be appreciated.

Tags (2)
0 Kudos
Reply
1 Reply

1,270 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please try to load the recent scfw package:

https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_SCFWKIT&appType=license&location=null 

Summary Page:

i.MX Software | NXP 

It contains documentation. Please refer to Chapter 3 (Porting Guide) of "sc_fw_port.pdf".


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply