Error when build images for IMX8 by Yocto project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error when build images for IMX8 by Yocto project

2,259件の閲覧回数
tangvubk
Contributor I

Hi all,

When following instructions in i.MX Yocto Project User's Guide to try to build images for my MCIMX8M-EVK KIT, I got an error with building package "libpam". A part of building log is attached below.

| aarch64-poky-linux-libtool: link: gcc -isystem/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/recipe-sysroot-native/usr/include -O2 -pipe -Wl,-rpath-link -Wl,/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/recipe-sysroot-native/usr/lib -Wl,-rpath-link -Wl,/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/recipe-sysroot-native/lib -Wl,-rpath -Wl,/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/recipe-sysroot-native/usr/lib -Wl,-rpath -Wl,/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/recipe-sysroot-native/lib -Wl,-O1 -o padout parse_l.o parse_y.o -L/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/recipe-sysroot-native/usr/lib -L/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/recipe-sysroot-native/lib
| parse_y.o: In function `yyparse':
| parse_y.c:(.text+0xc23): undefined reference to `__warn_memset_zero_len'
| collect2: error: ld returned 1 exit status
| Makefile:458: recipe for target 'padout' failed
| make[4]: *** [padout] Error 1
| make[4]: Leaving directory '/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/build/doc/specs'
| Makefile:411: recipe for target 'all' failed
| make[3]: *** [all] Error 2
| make[3]: Leaving directory '/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/build/doc/specs'
| Makefile:466: recipe for target 'all-recursive' failed
| make[2]: *** [all-recursive] Error 1
| make[2]: Leaving directory '/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/build/doc'
| Makefile:472: recipe for target 'all-recursive' failed
| make[1]: *** [all-recursive] Error 1
| make[1]: Leaving directory '/media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/build'
| Makefile:404: recipe for target 'all' failed
| make: *** [all] Error 2
| ERROR: oe_runmake failed
| WARNING: /media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/temp/run.do_compile.20204:1 exit 1 from 'exit 1'
| ERROR: Function failed: do_compile (log file is located at /media/vutt6/linuxwrk/imx8/fsl-arm-yocto-bsp/build-qt5/tmp/work/aarch64-poky-linux/libpam/1.3.0-r5/temp/log.do_compile.20204)

This error happens in my build machine run with Ubuntu 16.04.

Does anyone has any idea about what happen with my project?

Thank you very much.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,660件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please try adding the libpam package in the local.conf?

You can do it as below.

# gedit <your build directory>/conf/local.conf

Add the below at the end of the file:

IMAGE_INSTALL_append = " libpam"

Hope this can solve your problem.

Best regards,

Diego.

0 件の賞賛
返信