Error: oe_runmake failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error: oe_runmake failed

27,571 Views
yaşarcani_tişge
Contributor II

Hi,

I followed all the steps to make yocto image.
I get the following error during bitbake. How can i solve this error?

bitbake linux-imx -c compile -f 

then

ERROR: oe_runmake failed
ERROR: Function failed: do_compile (log file is located at /usr/IMX/fsl-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.14.52-r0/temp/log.do_compile.18054)
ERROR: Logfile of failure stored in: /usr/IMX/fsl-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.14.52-r0/temp/log.do_compile.18054
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 4 zImage CC=arm-poky-linux-gnueabi-gcc  -mno-thumb-interwork -marm -fuse-ld=bfd LD=arm-poky-linux-gnueabi-ld.bfd   LOADADDR=0x10008000
|   GEN     /usr/IMX/fsl-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.14.52-r0/build/Makefile
| scripts/kconfig/conf --silentoldconfig Kconfig
| *
| * Restart config...
| *
| *
| * Touchscreens
| *
| Touchscreens (INPUT_TOUCHSCREEN) [Y/n/?] y
|   ADS7846/TSC2046/AD7873 and AD(S)7843 based touchscreens (TOUCHSCREEN_ADS7846) [Y/n/m/?] y
|   AD7877 based touchscreens (TOUCHSCREEN_AD7877) [N/m/y/?] n
|   Analog Devices AD7879-1/AD7889-1 touchscreen interface (TOUCHSCREEN_AD7879) [N/m/y/?] n
|   Atmel mXT I2C Touchscreen (TOUCHSCREEN_ATMEL_MXT) [N/m/y/?] n
|   AUO in-cell touchscreen using Pixcir ICs (TOUCHSCREEN_AUO_PIXCIR) [N/m/y/?] n
|   BU21013 based touch panel controllers (TOUCHSCREEN_BU21013) [N/m/y/?] n
|   cy8ctmg110 touchscreen (TOUCHSCREEN_CY8CTMG110) [N/m/y/?] n
|   Cypress TTSP touchscreen (TOUCHSCREEN_CYTTSP_CORE) [N/m/y/?] n
|   Cypress TrueTouch Gen4 Touchscreen Driver (TOUCHSCREEN_CYTTSP4_CORE) [N/m/y/?] n
|   Dialog DA9052/DA9053 TSI (TOUCHSCREEN_DA9052) [N/m/y/?] n
|   Dynapro serial touchscreen (TOUCHSCREEN_DYNAPRO) [N/m/y/?] n
|   Hampshire serial touchscreen (TOUCHSCREEN_HAMPSHIRE) [N/m/y/?] n
|   EETI touchscreen panel support (TOUCHSCREEN_EETI) [N/m/y/?] n
|   EETI eGalax multi-touch panel support (TOUCHSCREEN_EGALAX) [Y/n/m/?] y
|   ELAN touchscreen input driver (TOUCHSCREEN_ELAN) [Y/n/m/?] y
|   Fujitsu serial touchscreen (TOUCHSCREEN_FUJITSU) [N/m/y/?] n
|   Goodix I2C touchscreen (TOUCHSCREEN_GOODIX) [N/m/y/?] (NEW) aborted!
|
| Console input/output is redirected. Run 'make oldconfig' to update configuration.
|
| /usr/IMX/fsl-bsp/build/tmp/work-shared/imx6qsabresd/kernel-source/scripts/kconfig/Makefile:36: recipe for target 'silentoldconfig' failed
| make[4]: *** [silentoldconfig] Error 1
| /usr/IMX/fsl-bsp/build/tmp/work-shared/imx6qsabresd/kernel-source/Makefile:514: recipe for target 'silentoldconfig' failed
| make[3]: *** [silentoldconfig] Error 2
| make[2]: *** No rule to make target 'include/config/auto.conf', needed by 'include/config/kernel.release'.  Stop.
| Makefile:133: recipe for target 'sub-make' failed
| make[1]: *** [sub-make] Error 2
| Makefile:26: recipe for target 'all' failed
| make: *** [all] Error 2
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /usr/IMX/fsl-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.14.52-r0/temp/log.do_compile.18054)
ERROR: Task 4 (/usr/IMX/fsl-bsp/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.52.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 258 tasks of which 257 didn't need to be rerun and 1 failed.

Labels (3)
4 Replies

15,504 Views
jmblanch
Contributor I

Hi, I have a similar problem.

After all these modifications when I go to build I see the following error:

I followed all the steps to make yocto image but i need support for fortran in my rootfs so i followed this:

[yocto] How do I enabled Fortran support in Sumo?

After all these modifications when I go to build I see the folloeing error:

| ERROR: Function failed: do_compile (log file is located at /home/t2080/QorIQ-SDK-V1.8-20150619-yocto/build_t2080rdb_release/tmp/work/ppce6500-fsl-linux/gcc/4.9.2-r0/temp/log.do_compile.18765)
ERROR: Task 720 (/home/t2080/QorIQ-SDK-V1.8-20150619-yocto/meta-fsl-toolchain/recipes-devtools/gcc/gcc_4.9.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3252 tasks of which 3233 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
/home/t2080/QorIQ-SDK-V1.8-20150619-yocto/meta-fsl-toolchain/recipes-devtools/gcc/gcc_4.9.bb, do_compile
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

I tried to clean the build but it doesn´t work.

Do you know how I can fix this?

0 Kudos
Reply

15,504 Views
gaurangk
Contributor I

Hi,

I am facing a similar issue(Error: "recipe for target 'silentoldconfig' failed") and I have tried to clean and build kernel image using below commands but it does to fix my issue.

$ bitbake linux-imx -c cleanall

$ bitbake linux-imx

Are there any fixes for this?

0 Kudos
Reply

15,504 Views
Yuri
NXP Employee
NXP Employee

Hello,

Please to try to clean previous built.

https://community.nxp.com/message/508584 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

15,504 Views
yaşarcani_tişge
Contributor II
Thank you for help 
Yasarcan 
0 Kudos
Reply