Error make mrproper in imx8m mini android 10 OS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error make mrproper in imx8m mini android 10 OS

1,629 次查看
Ruban1
Contributor II

Error make mrproper in imx8m mini android 10 OS

i have attached screenshot below

Thanks and regards

Ruban

0 项奖励
回复
2 回复数

1,624 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello  Ruban1,

 

At this point we can see that when there is a .config file in the kernel/ directory or a config/ directory exists in the kernel/include/ directory, the shell prints the error message seen at the beginning of this paragraph and exits. the problem is to delete the 2 objects. Go to the kernel/ directory and look for the .config file. If you go to the kernel/include/ directory, you will find the config/ directory! Go into the directory and see that it is empty (an empty directory can cause the entire project to fail to compile, and the details affect the success or failure!).

After removing the config/ directory, go back to the top of the Android project, re-execute the source and lunch commands, and recompile.

Regards

0 项奖励
回复

1,618 次查看
Ruban1
Contributor II

I am not able to find .config file.. the only file available is config.list.

Regard 

Ruban

0 项奖励
回复