iMX6ULL u-boot cannot recognize kernel image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6ULL u-boot cannot recognize kernel image

Jump to solution
3,100 Views
abdullahkahrama
Contributor IV

This question is a duplicate of:

https://community.nxp.com/t5/i-MX-Processors/iMX6ULL-u-boot-cannot-recognize-kernel-image/m-p/130687...

 

I have a custom board that I am trying to bring up. It passes the DDR stress tester over USB HID.

I have build an image according to i.MX_Yocto_Project_User's_Guide. My build configuration was:

MACHINE=imx6ullevk
DISTRO=fslc-framebuffer
IMAGE=core-image-minimal

I have then run dd command to burn .wic file to an SD card. The board boots up with SD card, however here is what I see on the terminal:

 

 

 

U-Boot 2020.10+fslc+g80c23498b4 (Mar 04 2021 - 17:46:24 +0000)                  
                                                                                
CPU:   Freescale i.MX6ULL rev1.1 900 MHz (running at 396 MHz)                   
CPU:   Commercial temperature grade (0C to 95C) at 48C                          
Reset cause: POR                                                                
Model: Freescale i.MX6 UltraLiteLite 14x14 EVK Board                            
Board: MX6ULL 14x14 EVK                                                         
DRAM:  512 MiB                                                                  
MMC:   FSL_SDHC: 0, FSL_SDHC: 1                                                 
Loading Environment from MMC... Card did not respond to voltage select!         
*** Warning - No block device, using default environment                        
                                                                                
In:    serial                                                                   
Out:   serial                                                                   
Err:   serial                                                                   
Net:   Could not get PHY for FEC1: addr 1                                       
Could not get PHY for FEC1: addr 1                                              
Could not get PHY for FEC0: addr 2                                              
Could not get PHY for FEC0: addr 2                                              
No ethernet found.                                                              
                                                                                
Normal Boot                                                                     
Hit any key to stop autoboot:  0                                                
Card did not respond to voltage select!                                         
Card did not respond to voltage select!                                         
Card did not respond to voltage select!                                         
Card did not respond to voltage select!                                         
Booting from net ...                                                            
Could not get PHY for FEC1: addr 1                                              
Could not get PHY for FEC1: addr 1                                              
Could not get PHY for FEC1: addr 1                                              
Could not get PHY for FEC0: addr 2                                              
Could not get PHY for FEC1: addr 1                                              
Could not get PHY for FEC1: addr 1                                              
No ethernet found.                                                              
Could not get PHY for FEC1: addr 1                                              
Could not get PHY for FEC1: addr 1                                              
Could not get PHY for FEC1: addr 1                                              
Could not get PHY for FEC1: addr 1                                              
Could not get PHY for FEC0: addr 2                                              
Could not get PHY for FEC1: addr 1                                              
Could not get PHY for FEC1: addr 1                                              
No ethernet found.                                                              
Could not get PHY for FEC1: addr 1                                              
zimage: Bad magic!                                                              
=>     

 

 

 

 

Then I try to read from the SD card, I wipe the DDR areas I am going to use, copy the zImage from the SD card to RAM, and check with iminfo and I get:

Unknown image format!

 

 

 

=>mmc info                                                                        
Device: FSL_SDHC                                                                
Manufacturer ID: 3                                                              
OEM: 5344                                                                       
Name: SU16G                                                                     
Bus Speed: 50000000                                                             
Mode: SD High Speed (50MHz)                                                     
Rd Block Len: 512                                                               
SD version 3.0                                                                  
High Capacity: Yes                                                              
Capacity: 14.8 GiB                                                              
Bus Width: 4-bit                                                                
Erase Group Size: 512 Bytes                                                     

=> mmc part                                                                     
                                                                                
Partition Map for MMC device 0  --   Partition Type: DOS                        
                                                                                
Part    Start Sector    Num Sectors     UUID            Type                    
  1     8192            53392           c2827fb8-01     0c Boot                 
  2     65536           40478           c2827fb8-02     83                      

=> ls mmc 0:1                                                                   
    30847   imx6ull-14x14-evk.dtb                                               
  7350040   zImage                                             
                                                                                
2 file(s)                                                           
                                                                                
=> md 82000000                                                                  
82000000: e1a00000 e1a00000 e1a00000 e1a00000    ................               
82000010: e1a00000 e1a00000 e1a00000 e1a00000    ................               
82000020: ea000003 016f2818 00000002 00702718    .....(o......'p.               
82000030: 04030201 e10f9000 eb0104f8 e1a07001    .............p..               
82000040: e1a08002 e10f2000 e3120003 1a000001    ..... ..........               
82000050: e3a20017 ef123456 e10f0000 a220001a    ....V4........ .               
82000060: e310001f e3c0001f e38000d3 1a000004    ................               
82000070: e3800c01 e28fe00c f16ff000 e12ef30e    ..........o.....               
82000080: f160206e e121f000 e16ff009 00000000    n `...!...o.....               
82000090: 02000000 00000000 00000000 00000000    ................               
820000a0: e1a0401f 6204433e e2844902 e1a0000f    .@..>C.b.I......               
820000b0: e1500084 349f01ac 3080000f 31540000    ..P....4...0..T1               
820000c0: 73844001 2300006d e28f0f5e e8901c4e    [email protected]..#^...N...               
820000d0: ed90d01c e0400001 e0866010 e082a000    ......@..`......               
820000e0: e5da9002 e5dae001 e189940e e5dac002    ................               
820000f0: e7daa003 e189980e e1899c0a e08dd000    ................               

=> mw 81000000 0 7000000                                                        

=> md 82000000                                                                  
82000000: 00000000 00000000 00000000 00000000    ................               
82000010: 00000000 00000000 00000000 00000000    ................               
82000020: 00000000 00000000 00000000 00000000    ................               
82000030: 00000000 00000000 00000000 00000000    ................               
82000040: 00000000 00000000 00000000 00000000    ................               
82000050: 00000000 00000000 00000000 00000000    ................               
82000060: 00000000 00000000 00000000 00000000    ................               
82000070: 00000000 00000000 00000000 00000000    ................               
82000080: 00000000 00000000 00000000 00000000    ................               
82000090: 00000000 00000000 00000000 00000000    ................               
820000a0: 00000000 00000000 00000000 00000000    ................               
820000b0: 00000000 00000000 00000000 00000000    ................               
820000c0: 00000000 00000000 00000000 00000000    ................               
820000d0: 00000000 00000000 00000000 00000000    ................               
820000e0: 00000000 00000000 00000000 00000000    ................               
820000f0: 00000000 00000000 00000000 00000000    ................               

=> load mmc 0:1 82000000 zImage                                                 
7350040 bytes read in 347 ms (20.2 MiB/s)                                       

=> md 82000000                                                                  
82000000: e1a00000 e1a00000 e1a00000 e1a00000    ................               
82000010: e1a00000 e1a00000 e1a00000 e1a00000    ................               
82000020: ea000003 016f2818 00000000 00702718    .....(o......'p.               
82000030: 04030201 e10f9000 eb0004f8 e1a07001    .............p..               
82000040: e1a08002 e10f2000 e3120003 1a000001    ..... ..........               
82000050: e3a00017 ef123456 e10f0000 e220001a    ....V4........ .               
82000060: e310001f e3c0001f e38000d3 1a000004    ................               
82000070: e3800c01 e28fe00c e16ff000 e12ef30e    ..........o.....               
82000080: e160006e e121f000 e16ff009 00000000    n.`...!...o.....               
82000090: 00000000 00000000 00000000 00000000    ................               
820000a0: e1a0400f e204433e e2844902 e1a0000f    .@..>C...I......               
820000b0: e1500004 359f01ac 3080000f 31540000    ..P....5...0..T1               
820000c0: 33844001 2b00006d e28f0f5e e8901c4e    [email protected]..+^...N...               
820000d0: e590d01c e0400001 e0866000 e08aa000    ......@..`......               
820000e0: e5da9000 e5dae001 e189940e e5dae002    ................               
820000f0: e5daa003 e189980e e1899c0a e08dd000    ................               

=> imi 82000000                                                                 
                                                                                
## Checking Image at 82000000 ...                                               
Unknown image format!                                                           

 

 

 

I have attached my zImage file. (I had to zip it since the forum doesn't accept a file without a type)

What could be my problem? 

Labels (2)
0 Kudos
Reply
1 Solution
3,077 Views
abdullahkahrama
Contributor IV

Seems like clue to the problem lays here:

mmcdev=1                                                                        
mmcpart=1                                                                       
mmcroot=/dev/mmcblk1p2 rootwait rw  

I am using mmc0 in my design, however I guess I need to configure it in uboot headers.

Setting these settings manually to mmc0, I can boot now, however "iminfo" still doesn't understand zImage. 

Thank you

View solution in original post

0 Kudos
Reply
2 Replies
3,078 Views
abdullahkahrama
Contributor IV

Seems like clue to the problem lays here:

mmcdev=1                                                                        
mmcpart=1                                                                       
mmcroot=/dev/mmcblk1p2 rootwait rw  

I am using mmc0 in my design, however I guess I need to configure it in uboot headers.

Setting these settings manually to mmc0, I can boot now, however "iminfo" still doesn't understand zImage. 

Thank you

0 Kudos
Reply
3,087 Views
JohnKlug
Senior Contributor I

My system boots, and imi also gives me unknown image format.  I am using raw nand and ubifs with a zImage.

=>printenv loadaddr
loadaddr=0x80800000
=> printenv bootcmd
bootcmd=run t_root;ubifsmount ubi0;ubifsload ${loadaddr} /boot/zImage;ubifsload ${fdt_addr} /boot/mtcap3.dtb;if test ${tee} = yes; then ubifsload ${tee_addr} /boot/uTee-6ullevk;bootm ${tee_addr} - ${fdt_addr};else bootz ${loadaddr} - ${fdt_addr};fi
=> ubifsmount ubi0
=> ubifsload ${loadaddr} /boot/zImage
Loading file '/boot/zImage' to addr 0x80800000...
Done
=> imi ${loadaddr}

## Checking Image at 80800000 ...
Unknown image format!
=> md $loadaddr 8
80800000: e1a00000 e1a00000 e1a00000 e1a00000    ................
80800010: e1a00000 e1a00000 e1a00000 e1a00000    ................


Does imi in U-Boot understand zImage?  Maybe it only understands uImage?

0 Kudos
Reply