Error in uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in uboot

1,940 Views
Ruban1
Contributor II

i2c i2c-0: IMX I2C adapter registered
[ 2.729439] gpio-146 (scl): enforced open drain please flag it properly in DT/ACPI DSDT/board file
[ 2.739252] imx8mm-pinctrl 30330000.pinctrl: pin MX8MM_IOMUXC_NAND_ALE already requested by 30bb0000.spi; cannot claim for 1-002c
[ 2.750922] imx8mm-pinctrl 30330000.pinctrl: pin-61 (1-002c) status -22
[ 2.757549] imx8mm-pinctrl 30330000.pinctrl: could not request pin 61 (MX8MM_IOMUXC_NAND_ALE) from group lvdsgrp on device 30330000.pinctrl
[ 2.770164] sn65dsi83 1-002c: Error applying setting, reverse things back
[ 2.776973] sn65dsi83: probe of 1-002c failed with error -22

Can you help me where to config to disable where it is used

Labels (1)
0 Kudos
Reply
1 Reply

1,908 Views
Juan-Rodarte
NXP Employee
NXP Employee

Hello,

I noticed that you have opened other threads that are related to the same problem, if possible I would like to keep communication in one thread so we can avoid any misunderstanding.

https://community.nxp.com/t5/i-MX-Processors/U-boot-error-In-IMX8M-MINI-EVK-for-Android-10-OS/td-p/1...

Regards,

Diego.

0 Kudos
Reply