Error in meta-toolchain-qt with linux 2.6.35.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in meta-toolchain-qt with linux 2.6.35.3

3,025件の閲覧回数
tonim
Contributor I

Hello.

I'm trying integrate Qt4 with Yocto dizzy 1.7.1.

When execute this command:

bitbake meta-toolchain-qt


Return this error:


ERROR: Task do_configure in /home/sopra/poky/meta/recipes-qt/qt4/qt4-x11-free_4.8.6.bb depends upon non-existent task do_shared_workdir in /home/sopra/meta-fsl-arm/recipes-kernel/linux/linux-imx_2.6.35.3.bb

My configuration is:

Build Configuration:

BB_VERSION        = "1.24.0"

BUILD_SYS         = "i686-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx51evk"

DISTRO            = "poky"

DISTRO_VERSION    = "1.7.1"

TUNE_FEATURES     = "arm armv7a vfp neon"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "dizzy:ec75238f6cc2d2d8d40e0268f6d2acc070cbe9a4"

meta-fsl-arm      = "master:0b3457e7160a0069bb933558034a749b042bba88"

This is for a imx51evk machine with linux 2.6.35.3

Any idea what happens?

Thanks.

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

2,444件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Have you posted this question in meta-freescale?

0 件の賞賛
返信

2,444件の閲覧回数
DraganOstojic
Contributor V

Hi Diane, I know you are the Yocto expert for IMX6. I have another problem with this same command. Can you please check my post:

https://community.freescale.com/thread/352770

0 件の賞賛
返信

2,444件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I don't have access to the link you shared

0 件の賞賛
返信

2,444件の閲覧回数
DraganOstojic
Contributor V

Sorry for that. I corrected the link:

https://community.freescale.com/thread/352770

0 件の賞賛
返信

2,444件の閲覧回数
tonim
Contributor I

The problem is in qt4-imx-support.inc file in meta-fsl-arm/recipies-qt/qt:

FILESEXTRAPATHS_prepend := "${THISDIR}/qt4:"

python __anonymous () {

    families = ['mx5', 'mx6']

    cur_families = (d.getVar('SOC_FAMILY', True) or '').split(':')

    if any(map(lambda x: x in cur_families,

              families)):

        d.appendVarFlag('do_configure', 'depends', ' virtual/kernel:do_shared_workdir')

}

SRC_URI_append_mx5 += "file://0001-Add-support-for-i.MX-codecs-to-phonon.patch"

SRC_URI_append_mx6 += " \

    file://0001-Add-support-for-i.MX-codecs-to-phonon.patch \

    file://0002-i.MX-video-renderer-Allow-v4l-device-from-environmen.patch \

    file://0003-i.MX6-force-egl-visual-ID-33.patch \

"

DEPENDS_append_mx5 = " virtual/kernel virtual/libgles2"

QT_GLFLAGS_mx5 = "-opengl es2 -openvg"

QT_CONFIG_FLAGS_append_mx5 = " -I${STAGING_KERNEL_DIR}/include/"

DEPENDS_append_mx6 = " virtual/kernel virtual/libgles2"

QT_GLFLAGS_mx6 = "-opengl es2 -openvg"

QT_CONFIG_FLAGS_append_mx6 = " -I${STAGING_KERNEL_DIR}/include/uapi \

                              -I${STAGING_KERNEL_DIR}/include/ \

                              -DLINUX=1 -DEGL_API_FB=1 \

                              -DQT_QPA_EXPERIMENTAL_TOUCHEVENT=1"

I comment this lines ¿is correct?.


Thanks.

0 件の賞賛
返信

2,444件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

The problem is the missing task in the kernel source code.

When you comment that line, you are only avoiding a dependence. Maybe it works, maybe not (determinism, schedule, this kind of probability)

The right way to fix it is to add the do_shared_workdir in kernel recipe


More than that I would need to debug the issue.

0 件の賞賛
返信