Error in dts mappings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in dts mappings

1,203 Views
amitkulkarni
Contributor II

When i do

dmesg | grep -i bt

i'm getting following msg:

imx6q-pinctrl 20e0000.iomuxc: unable to find group for node btreggrp

What coould be the reason for it ? How to resolve it ?

Board: Toradex apalisx ixora imx6q

OS: Android 7.0

dts files are attached below.

Labels (2)
0 Kudos
Reply
1 Reply

1,097 Views
igorpadykov
NXP Employee
NXP Employee

Hi Amit

one can try to rebuild image anew from scratch or try with nxp release

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply