Error in dts mappings

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error in dts mappings

1,590 次查看
amitkulkarni
Contributor II

When i do

dmesg | grep -i bt

i'm getting following msg:

imx6q-pinctrl 20e0000.iomuxc: unable to find group for node btreggrp

What coould be the reason for it ? How to resolve it ?

Board: Toradex apalisx ixora imx6q

OS: Android 7.0

dts files are attached below.

标签 (2)
标记 (5)
0 项奖励
回复
1 回复

1,484 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Amit

one can try to rebuild image anew from scratch or try with nxp release

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复