Error compiling Python 2.7 using LTIB for iMX35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error compiling Python 2.7 using LTIB for iMX35

9,225 Views
neo1
Contributor II

Hey,

Has anyone compiled python 2.7 using LTIB for imx35?

I have attached the spec file

These are the errors I get:

In file included from Include/Python.h:58,

                 from ./Modules/python.c:3:

Include/pyport.h:243:13: error: #error "This platform's pyconfig.h needs to define PY_FORMAT_LONG_LONG"

In file included from Include/Python.h:58,

                 from Parser/grammar1.c:4:

Include/pyport.h:243:13: error: #error "This platform's pyconfig.h needs to define PY_FORMAT_LONG_LONG"

In file included from Include/Python.h:58,

                 from Include/pgenheaders.h:10,

                 from Parser/acceler.c:13:

Include/pyport.h:243:13: error: #error "This platform's pyconfig.h needs to define PY_FORMAT_LONG_LONG"

In file included from Include/Python.h:58,

                 from Parser/node.c:3:

Include/pyport.h:243:13: error: #error "This platform's pyconfig.h needs to define PY_FORMAT_LONG_LONG"

In file included from Include/Python.h:58,

                 from Parser/parser.c:8:

Include/pyport.h:243:13: error: #error "This platform's pyconfig.h needs to define PY_FORMAT_LONG_LONG"

In file included from Include/Python.h:58,

                 from Include/pgenheaders.h:10,

                 from Parser/listnode.c:4:

Include/pyport.h:243:13: error: #error "This platform's pyconfig.h needs to define PY_FORMAT_LONG_LONG"

In file included from Include/Python.h:58,

                 from Include/pgenheaders.h:10,

                 from Parser/bitset.c:4:

Include/pyport.h:243:13: error: #error "This platform's pyconfig.h needs to define PY_FORMAT_LONG_LONG"

In file included from Include/Python.h:58,

                 from Include/pgenheaders.h:10,

                 from Parser/parsetok.c:4:

Include/pyport.h:243:13: error: #error "This platform's pyconfig.h needs to define PY_FORMAT_LONG_LONG"

make: *** [Modules/python.o] Error 1

I used the build commands spec file from this link

Re: [Ltib] Building Python 2.7

 

I don't understand if this error is related to the python source or the arm tools used by ltib. Can someone please help?

Has anyone compiled python successfully? if so, what am I doing wrong?

Original Attachment has been moved to: Python-2.7.3.spec.zip

Labels (1)
Tags (1)
0 Kudos
Reply
7 Replies

5,894 Views
LeonardoSandova
Specialist I

It is not the same problem but try the proposed solution on this link

Re: "FSL gnome release package" build fails at python build stage

5,893 Views
neo1
Contributor II

Thanks Leonardo,

Unfortunately that did not work.

I made an interesting observation tho. I looked at the output of the ./configure scripts that created the makefiles.

checking size of size_t... 4

checking size of pid_t... 4

checking for long long support... yes

checking size of long long... 8

checking for long double support... yes

So if it does have support for long long, y doesn't it compile??

0 Kudos
Reply

5,893 Views
LeonardoSandova
Specialist I

Hi Neeraj,

http://www.cnx-software.com/2011/02/04/cross-compiling-python-for-mips-and-arm-platforms/

I think you are not the only one with this issue, but there is patch to solve it. Pyhon on LTIB is on rpm/BUILD/<python> so apply the patch from that folder.

5,893 Views
neo1
Contributor II

Hi Leonardo,

Thanks for the link.

I got sidetracked on other projects and wasnt able to follow up.

After using the patch I dont get the PY_FORMAT_LONG_LONG error any more.

However,

I get a ton of warning messages and python builds but with some key modules missing.

cc1: warning: include location "/usr/include" is unsafe for cross-compilation

cc1: warning: include location "/usr/local/include" is unsafe for cross-compilation

cc1: warning: include location "/usr/include" is unsafe for cross-compilation

cc1: warning: include location "/usr/local/include" is unsafe for cross-compilation

/home/neeraj/Development/Freescale/ltib/rpm/BUILD/Python-2.7.1/Modules/_ctypes/libffi/src/arm/ffi.c:205: warning: function declaration isn't a prototype

/opt/freescale/usr/local/gcc-4.3.3-glibc-2.8-cs2009q1-203/arm-none-linux-gnueabi/bin/../lib/gcc/arm-none-linux-gnueabi/4.3.3/../../../../arm-none-linux-gnueabi/bin/ld: warning: library search path "/usr/local/lib" is unsafe for cross-compilation

*** WARNING: renaming "_ctypes" since importing it failed: build/lib.linux-i686-2.7/_ctypes.so: cannot open shared object file: No such file or directory

Python build finished, but the necessary bits to build these modules were not found:

_bsddb             _hashlib           _sqlite3       

_tkinter           bsddb185           dbm            

gdbm               sunaudiodev                       

To find the necessary bits, look in setup.py in detect_modules() for the module's name.

Failed to build these modules:

_multiprocessing   _socket            linuxaudiodev  

ossaudiodev        readline           select         

+ exit 0

Build time for Python-2.7.1: 128 seconds

Line 356 and 357 have hardcoded /usr/local/include and /usr/local/lib

Also get errors like these higher up.

*** WARNING: renaming "dl" since importing it failed: build/lib.linux-i686-2.7/dl.so: cannot open shared object file: No such file or directory

cc1: warning: include location "/usr/include" is unsafe for cross-compilation

cc1: warning: include location "/usr/local/include" is unsafe for cross-compilation

cc1: warning: include location "/usr/include" is unsafe for cross-compilation

cc1: warning: include location "/usr/local/include" is unsafe for cross-compilation

/home/neeraj/Development/Freescale/ltib/rpm/BUILD/Python-2.7.1/Modules/_multiprocessing/connection.h: In function 'connection_poll':

/home/neeraj/Development/Freescale/ltib/rpm/BUILD/Python-2.7.1/Modules/_multiprocessing/socket_connection.c:173: error: impossible constraint in 'asm'

cc1: warning: include location "/usr/include" is unsafe for cross-compilation

cc1: warning: include location "/usr/local/include" is unsafe for cross-compilation

/home/neeraj/Development/Freescale/ltib/rpm/BUILD/Python-2.7.1/Modules/linuxaudiodev.c: In function 'lad_write':

/home/neeraj/Development/Freescale/ltib/rpm/BUILD/Python-2.7.1/Modules/linuxaudiodev.c:192: error: impossible constraint in 'asm'

cc1: warning: include location "/usr/include" is unsafe for cross-compilation

cc1: warning: include location "/usr/local/include" is unsafe for cross-compilation

/home/neeraj/Development/Freescale/ltib/rpm/BUILD/Python-2.7.1/Modules/ossaudiodev.c: In function 'oss_writeall':

/home/neeraj/Development/Freescale/ltib/rpm/BUILD/Python-2.7.1/Modules/ossaudiodev.c:429: error: impossible constraint in 'asm'

0 Kudos
Reply

5,893 Views
LeonardoSandova
Specialist I

You are compiling python with ltib, right? something like './ltib -p python -scbuild' ? Seems that the header files are being taken from the host filesystem, instead of the ltib filesystem..

0 Kudos
Reply

5,891 Views
neo1
Contributor II

Yes I am using ./ltib -p Python-2.7.1.spec -m scbuild

Attaching the spec file. I have changed the spec file after going thru some of the above links.

What am I doing wrong here?

0 Kudos
Reply

5,891 Views
LeonardoSandova
Specialist I

Hi neo1, could you please generate a patch instead of the whole .spec? try this

$ cd <original spec folder>

$ git init

$ git add *.spec

$ git commit -m 'first commit'

$ # do your changes here

$ git commit -a -m 'changes'

$ git format-patch -1

then send me the generated .patch file please.

0 Kudos
Reply