Error adding new packages on ltib

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error adding new packages on ltib

1,201件の閲覧回数
unaigonzalez
Contributor II

i want to add olsrd to the packages list, to build it in to the imx28evk using ltib.

I followed the next steps:

1. copy source in /opt/freescale/pkgs

2. create file source_name.md5

md5sum source_name > source_name.md5

3. create directory in <you_ltib_dir>dist/lfs-5.1/<you_package> and copy spec-file to it

After this you can use ltib for build package:

1. ./ltib -m prep -p package.spec

2. ./ltib -m scbuild -p package.spec

3. ./ltib -m scdeploy -p package.spec

i also added on config/userspace/packages.lkc (alphabetic order)

      config PKG_OLSRD

           bool "olsrd"

and on config/userspace/pkg_map (build order)

       PKG_OLSRD = olsrd

but, when i execute the comand:

./ltib -m prep -p olsrd.spec

this error appear:

plc@ubuntu:~/ltib$ ./ltib -m prep -p olsrd.spec

Processing: olsrd

===================

Build path taken because: build key set, no prebuilt rpm,

Testing network connectivity

OK GPP:

Try olsrd-current.tar.bz2.md5 from the GPP

http://bitshrine.org/gpp/olsrd-current.tar.bz2.md5:

06:25:58 ERROR 404: Not Found.

Try olsrd-current.tar.bz2 from the GPP

http://bitshrine.org/gpp/olsrd-current.tar.bz2:

06:25:58 ERROR 404: Not Found.

Can't get: olsrd-current.tar.bz2 at ./ltib line 790.

f_prep() returned an error, exiting

traceback:

main:560

Exiting on error or interrupt

I know that olsrd is not able at gpp, but i thought this was enought to found it on ppp or lpp, i think im missing something, but i dont know what.

Thanks for the help.

ラベル(1)
0 件の賞賛
返信
1 返信

922件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

It is possible that the .librc is not configured with the necessary options in order to download the file from a local repository. Do you have the olsrd-current.tar.bz2 file on the rmp/SOURCES path ?

I would recommend reading the following link on the “Where do the sources get downloaded from (what is the LPP/GPP/PPP)” section for information on how the download is handled when it cannot be downloaded.

http://www.bitshrine.org/autodocs/LtibFaq.html

0 件の賞賛
返信