Dear all,
We see Ordering information of i.MX6SoloX.
The following document is referred to.
- IMX6SXAEC.pdf (Rev0)
- IMX6SXCEC.pdf (Rev0)
- IMX6SXIEC.pdf (Rev0)
Some descriptions of Option of the "Table 1. Ordering information" are different from "Figure 1. Part Number Nomenclature-i.MX 6SoloX".
[1]
In teh Part differentiator "2" of Figure 1, ADC is not supported.
However, in the option of Table 1, ADC is not included in "Features not supported:"
(In other words, the ADC is supported.)
Which is right?
[2]
In teh Part differentiator "3" of Figure 1, Package VN is not supported the ADC.
However, in the option of Table 1, ADC is not included in "Features not supported:"
Which is right?
Best Regards,
Yuuki