Enviroment setup for uboot and linux kernel build in imx8m plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enviroment setup for uboot and linux kernel build in imx8m plus

Jump to solution
1,451 Views
Jimmychea
Contributor III

The eviromement setup for uboot and linux kernel build are same using below command ?

source /opt/fsl-imx-xwayland/5.15-kirkstone/environment-setup-armv8a-poky-linux

Labels (1)
0 Kudos
Reply
1 Solution
1,437 Views
Jimmychea
Contributor III
0 Kudos
Reply
2 Replies
1,438 Views
Jimmychea
Contributor III

Thanks

0 Kudos
Reply
1,441 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, the same toolchain /opt/fsl-imx-wayland/5-15-kirkstone/environment-setup-xxx