Encrypt filesystem on NAND

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Encrypt filesystem on NAND

3,612 Views
mirkoardinghi1
Contributor IV

Hi, I need to encrypt the filesystem on NAND (ubifs) on iMX6

Is there any documentation?

 

Labels (4)
Tags (1)
0 Kudos
Reply
3 Replies

3,600 Views
mirkoardinghi1
Contributor IV

Hi Igor.

I read AN12714

In chapter 3 is wrote:

"NAND flash is an MTD device, hence, DM-Crypt cannot be used with it and the hands-on do not apply for it."

So the question is: "How can I encrypt NAND on iMX6"?

0 Kudos
Reply

3,586 Views
igorpadykov
NXP Employee
NXP Employee

answer from team below:

-----------------

Yes, dm-crypt can't directly be used on MTD device. It seems like that customer can use fscrypt[1] with UBIFS

 

[1]https://www.kernel.org/doc/html/latest/filesystems/fscrypt.html

-----------------

Best regards
igor

0 Kudos
Reply

3,603 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply