Encrypt filesystem on NAND

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Encrypt filesystem on NAND

3,639件の閲覧回数
mirkoardinghi1
Contributor IV

Hi, I need to encrypt the filesystem on NAND (ubifs) on iMX6

Is there any documentation?

 

ラベル(4)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

3,627件の閲覧回数
mirkoardinghi1
Contributor IV

Hi Igor.

I read AN12714

In chapter 3 is wrote:

"NAND flash is an MTD device, hence, DM-Crypt cannot be used with it and the hands-on do not apply for it."

So the question is: "How can I encrypt NAND on iMX6"?

0 件の賞賛
返信

3,613件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

answer from team below:

-----------------

Yes, dm-crypt can't directly be used on MTD device. It seems like that customer can use fscrypt[1] with UBIFS

 

[1]https://www.kernel.org/doc/html/latest/filesystems/fscrypt.html

-----------------

Best regards
igor

0 件の賞賛
返信

3,630件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信