Encrypt filesystem on NAND

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Encrypt filesystem on NAND

2,794 次查看
mirkoardinghi1
Contributor IV

Hi, I need to encrypt the filesystem on NAND (ubifs) on iMX6

Is there any documentation?

 

标签 (4)
标记 (1)
0 项奖励
回复
3 回复数

2,782 次查看
mirkoardinghi1
Contributor IV

Hi Igor.

I read AN12714

In chapter 3 is wrote:

"NAND flash is an MTD device, hence, DM-Crypt cannot be used with it and the hands-on do not apply for it."

So the question is: "How can I encrypt NAND on iMX6"?

0 项奖励
回复

2,768 次查看
igorpadykov
NXP Employee
NXP Employee

answer from team below:

-----------------

Yes, dm-crypt can't directly be used on MTD device. It seems like that customer can use fscrypt[1] with UBIFS

 

[1]https://www.kernel.org/doc/html/latest/filesystems/fscrypt.html

-----------------

Best regards
igor

0 项奖励
回复

2,785 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复