Encountered several problems when using Vivante tools to analyze .vpd files generated by vprofiler

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Encountered several problems when using Vivante tools to analyze .vpd files generated by vprofiler

1,757 次查看
wangyuan
Contributor I

The development environment is imx6q platform, linux kernel version is 3.14.52.

When I use the vProfiler tool to test gpu utilization (the .vpd files generated by vProfiler and use vAnalyzer to view vpd files), encountered several problems as follows:

1.Running the samples in viv_samples/vdk coming with kernel 3.14.52, there is only 1 .vpd files generated.

However, running my simple Qt program(using QOpenGLWidget), there are 4 .vpd files generated, 2 of them contain only 1 frame and the other 2 contain expected number of frames. Why are there multiple .vpd files generated?

捕获.PNG

2. between the 2 "valid" .vpd file mentiond at 1,  gpu utilization is different, one is big(over 80%) and the other is small (below 30%), and the addition of the 2 gpu utilization value is bigger than 100%(why?) 

RTX截图未命名1.png

RTX截图未命名2.png

3. what does driver utilization mean ? Actully, I also want to known the exact meaning of gpu utilization because of the above question.

Thanks in advance!

0 项奖励
回复
2 回复数

1,644 次查看
wangyuan
Contributor I

Do you have a similar problem?

Waiting for help!

Thank you!

0 项奖励
回复

1,644 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复