Dear Team,
SW: Android Automotive 13.0.0_1.1.0
HW: iMX8QM MEK
Application core : Android
M4 core : Free RTOS
Please refer the below table.
I need to run below requirements simultaneously.
Requirement 1: I need to drive 2 displays from Android (LVDS0_CH0, MIPI_DSI1)
Requirement 2: I need to drive 2 displays from FreeRTOS (HDMI_TX, LVDS1_CH0)
Is it possible? If so, can you help with the changes required.
Reference : 8.3.2 Enabling multiple-display function
| Board | Number of displays | Display port |
| i.MX 8QuadMax MEK | 4 | HDMI_TX, LVDS0_CH0, LVDS1_CH0, MIPI_DSI1 |
| Optional | 4 | LVDS0_CH0 and LVDS1_CH0, MIPI_DSI0 and MIPI_DSI1 |
Best regards
Jose.