Enabling MII interface in sabreAI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling MII interface in sabreAI

2,008 Views
rahulramakrishn
Contributor III

Hi

I wan't to enable the MII interface in the sabreai board. Is MII interface is supported in the sabreai? How can I get the schematics for the sabreai?

regards

Rahul Ramakrishnan 

0 Kudos
Reply
2 Replies

1,893 Views
Yuri
NXP Employee
NXP Employee

Hello,

   RGMII is used on the SABRE AI boards. MII cannot be configured there because of

different set of pins.

Summary page:

SABRE|Automotive-Infotainment|i.MX6|NXP 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,893 Views
rahulramakrishn
Contributor III

Thank you for the information.

0 Kudos
Reply