Enabling MII interface in sabreAI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enabling MII interface in sabreAI

2,022 次查看
rahulramakrishn
Contributor III

Hi

I wan't to enable the MII interface in the sabreai board. Is MII interface is supported in the sabreai? How can I get the schematics for the sabreai?

regards

Rahul Ramakrishnan 

0 项奖励
回复
2 回复数

1,907 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   RGMII is used on the SABRE AI boards. MII cannot be configured there because of

different set of pins.

Summary page:

SABRE|Automotive-Infotainment|i.MX6|NXP 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,907 次查看
rahulramakrishn
Contributor III

Thank you for the information.

0 项奖励
回复