Enabling Cache for display module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling Cache for display module

1,398件の閲覧回数
EmbeddedTech
Contributor III

Hi,

I would like to know how disabling the cache (SCB_DisableDCache()) will affect the performance of the LCD display. If I disable the cache the update gets slower. On enabling cache the display update is faster but the pixels are not updated properly on the first refresh when a screen is changed. Also the USB host functionality does not enumerate the mouse if cache is enabled. How to solve this issue?

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,376件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the application note to learn the cache feature, further, the application note also guides users on how to use cache to develop applications running in a correct and high-performance way.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信