Enabling Cache for display module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling Cache for display module

1,436 Views
EmbeddedTech
Contributor III

Hi,

I would like to know how disabling the cache (SCB_DisableDCache()) will affect the performance of the LCD display. If I disable the cache the update gets slower. On enabling cache the display update is faster but the pixels are not updated properly on the first refresh when a screen is changed. Also the USB host functionality does not enumerate the mouse if cache is enabled. How to solve this issue?

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,414 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the application note to learn the cache feature, further, the application note also guides users on how to use cache to develop applications running in a correct and high-performance way.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply