Enable ethernet Wake-On-LAN feature on i.MX8 with Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable ethernet Wake-On-LAN feature on i.MX8 with Android

3,175 Views
yyc1975
Contributor III

Hi All,

We can enable WoL feature on Yocto linux and wakeup device from suspend.

It fails to wakeup system when change to Android.

Did anyone knows how to enable WoL feature on Android OS?

Best Regards,

YY

0 Kudos
Reply
5 Replies

3,078 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which android BSP are you using?

0 Kudos
Reply

3,078 Views
yyc1975
Contributor III

Hi b45499,

We are using Android P9.0.0_2.3.2 (Linux 4.14 kernel) Android P9.0.0_2.3.4-patch.

SoC: I.MX8MQ and I.MX8MD

Android_release.PNG

Best Regards,

YY

0 Kudos
Reply

3,078 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

P9.0.0_2.3.2.PNG

This version is only for i.MX8MN and i.MX8QXP, if you are use the i.MX8M series you can try other version.

0 Kudos
Reply

3,078 Views
yyc1975
Contributor III

Hi b45499‌,

We have built our own board with i.MX8MQ and i.MX8MD SoC not EVK.

We use "Android P9.0.0_2.3.2 (Linux 4.14 kernel) Android P9.0.0_2.3.4-patch" as code base of our BSP and added our drivers and modifications.

Is that necessary to use "Correct version BSP" for specific SoC?

For the WOL issue, it should be common issue for any i.MX SoC, isn't it?

Best Regards,

YY

0 Kudos
Reply

3,078 Views
yyc1975
Contributor III

HI b45499‌,

Do you have any idea about the WOL feature on Android platform?

Thanks!

YY

0 Kudos
Reply