Enable PCI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable PCI

4,632件の閲覧回数
niklasmolin
Senior Contributor I

I'm trying to use the PCI bus to communicate with a FPGA.

In the device tree I had to disabled the PCI bus during bootup, since it got stuck during bootup because the PCI bus could not link up (EP mode).

The FPGA won't be loaded until the Linux is booted up, how do I enable the PCI "driver" after the kernel is up and running?

Thanks,

Niklas

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

4,445件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

please check sect.40.2.2 Kernel Configurations

attached Linux Manual. Note, PCI Express support can't be built as a module.

May be useful links

i.mx6q pcie cannot recognize i210 

IMX6Q: Linux boot halts at PCIe config space read 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,445件の閲覧回数
niklasmolin
Senior Contributor I

Hi Igor.

When I tried to klick on the first link I got following error:

Unauthorized

This place or content does not exist or access to it is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.

Best regards,

Niklas

0 件の賞賛
返信

4,445件の閲覧回数
niklasmolin
Senior Contributor I

Hi Igor.

Thanks for the response.

I'll check the provided info.

Best regards,

Niklas

0 件の賞賛
返信