Enable CAAM in imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable CAAM in imx6q

1,649 Views
yilingxu
Contributor III

Hi,

I want to enable CAAM in linux. I have two questions:

1. How to enable CAAM in linux directly, without passing parameter from uboot bootargs?

2. How to determine CAAM is enabled or not? eg. If I enable the CAAM, what should I see in "/dev"?

Thanks,

Yiling Xu

Labels (2)
0 Kudos
Reply
1 Reply

1,478 Views
igorpadykov
NXP Employee
NXP Employee

Hi

1. please check sect.8.1.6 Driver Configuration attached Linux Manual.

2. one can try caam unit test

caam\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply