i.MX8M / i.MX8X support QSPI/FlexSPI slave mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M / i.MX8X support QSPI/FlexSPI slave mode

1,219 Views
andychien
Contributor III

Dear Sir,

Our customer want to use QSPI/FlexSPI slave mode on NXP i.MX8M / i.MX8X platform.

The architecture is FPGA QSPI/FlexSPI master  and  i.MX8M / i.MX8X QSPI/FlexSPI  is slave.

We don't see more support information on datasheet or reference manual.

Could you help check and confirm it?

Thanks,

0 Kudos
1 Reply

789 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

for spi slave protocols these processors have ecspi, lpspi modules,

as for qspi/flexspi modules, for them spi slave mode is not supported, based on

documentation.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos