Embedded linux and i.mx books.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Embedded linux and i.mx books.

ソリューションへジャンプ
9,617件の閲覧回数
ssinfod
Contributor IV

Hello,

I want to use embedded Linux (yocto) on the i.mx 6 processor. I already booted some dev kit with yocto on it.

Now, I'm looking for some text book that explains how to use the peripheral of the i.mx 6 with Linux. (For example: SPI, I2C, Timer, ATD, Timer, CAN, UART, etc.)

I'm coming from the microcontroller world (Freescale HCS08, HCS12, etc..) and I am a little lost regarding these subjects.

Can anyone suggest me some good text books or tutorial on how to use the i.mx peripheral inside Linux ?

Thanks

ssinfod

ラベル(5)
1 解決策
8,550件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

You can find the path of the driver source code in i.MX6 Linux Reference Manual.

For the example on how to use it, you can take the imx-test for reference. (<Yocto_BuildDir>/imx-test-"version")

元の投稿で解決策を見る

5 返答(返信)
8,550件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
8,550件の閲覧回数
ssinfod
Contributor IV

Thanks, I ordered and read that book already. It gives a good overview of yocto but I would like more examples on how to use the feature of the i.mx processor.

ssinfod

0 件の賞賛
返信
8,544件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I think the Linux reference manual and the porting guide in the Yocto BSP documentation are useful for you.

0 件の賞賛
返信
8,544件の閲覧回数
ssinfod
Contributor IV

Thanks these documents seems to contains a lot of usefull information.

One last question..

Can you explain to me one last thing. With Freescale MCU, I'm used to write the driver code myself. For example, I could set and get the UART registers (SCI0BD, SCI0DR), baud rate, data bits, etc..

With the Linux (yocto), who is writing the driver for the i.mx ? Is it the Freescale team or the Linux team ?

Where can I see the code for the i.mx peripheral drivers ? (Timer, UART, SPI, I2C) ?

In fact, I would like to see the i.mx peripheral driver code and also example on how to use it.

ssinfod

0 件の賞賛
返信
8,551件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

You can find the path of the driver source code in i.MX6 Linux Reference Manual.

For the example on how to use it, you can take the imx-test for reference. (<Yocto_BuildDir>/imx-test-"version")