Editing /ueventd.rc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Editing /ueventd.rc

3,703 Views
PaulMcGregor
Contributor I

I an trying to edit /ueventd.rc to add the line

 "/dev/ttymxc0 0666 root root"

allowing normal users access to the com port.

 

I have remounted the rootfs as read write and pushed the updated file however after cycling power  the changes are gone.

 

Any help would be appreciated. 

Labels (1)
0 Kudos
Reply
2 Replies

1,938 Views
daiane_angolini
NXP Employee
NXP Employee
you can see how to modify uramdisk.img on User Guide. Search for "cpio"
0 Kudos
Reply

1,938 Views
AlanLevy
Contributor I

The root is a RAM file system so all changes are lost at reboot. To make permanent changes you need to modify the contents of uramdisk.img and put that onto the boot device, which has to be done from a host development system.

0 Kudos
Reply