Editing /ueventd.rc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Editing /ueventd.rc

4,292件の閲覧回数
PaulMcGregor
Contributor I

I an trying to edit /ueventd.rc to add the line

 "/dev/ttymxc0 0666 root root"

allowing normal users access to the com port.

 

I have remounted the rootfs as read write and pushed the updated file however after cycling power  the changes are gone.

 

Any help would be appreciated. 

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,527件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee
you can see how to modify uramdisk.img on User Guide. Search for "cpio"
0 件の賞賛
返信

2,527件の閲覧回数
AlanLevy
Contributor I

The root is a RAM file system so all changes are lost at reboot. To make permanent changes you need to modify the contents of uramdisk.img and put that onto the boot device, which has to be done from a host development system.

0 件の賞賛
返信