Editing init.rc file after boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Editing init.rc file after boot

1,690 次查看
lyfsci
Contributor III

Hi Experts,

I would like to edit the init.rc file and let it be saved permanently. But during each restart of the machine the init.rc file is the same as I build.

How to solve the same ?

Regards,

Lyf

标签 (1)
0 项奖励
回复
2 回复数

1,560 次查看
tomgao
Contributor III

could you introduce how to update the initramfs cpio ?

0 项奖励
回复

1,560 次查看
b36401
NXP Employee
NXP Employee

Does you system run on root filesystem unpacked from ramdisk?

In this case you need to update the file inside of initramfs cpio archive.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复