Editing init.rc file after boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Editing init.rc file after boot

1,691件の閲覧回数
lyfsci
Contributor III

Hi Experts,

I would like to edit the init.rc file and let it be saved permanently. But during each restart of the machine the init.rc file is the same as I build.

How to solve the same ?

Regards,

Lyf

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,561件の閲覧回数
tomgao
Contributor III

could you introduce how to update the initramfs cpio ?

0 件の賞賛
返信

1,561件の閲覧回数
b36401
NXP Employee
NXP Employee

Does you system run on root filesystem unpacked from ramdisk?

In this case you need to update the file inside of initramfs cpio archive.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信