ESAI for SPDIF receiver usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ESAI for SPDIF receiver usage

1,859件の閲覧回数
xkwy
Contributor I

Hi,

I'm using i.MX 6ULL for audio encoder product, Its need two SPDIF receive interface.

But i.MX only have one origin SPDIF receiver. I'm looking for ESAI to handle this.

 

as the ESAI document says:

The Enhanced Serial Audio Interface (ESAI) provides a full-duplex serial port for serial communication with a variety of serial devices, including industry-standard codecs, Sony/Phillips Digital Interface (SPDIF) transceivers, and other DSPs.

 

My question is: Does ESAI can working on SPDIF receiver mode and working together with i.MX's origin SPDIF(receiver), and any sample code for reference?

0 件の賞賛
返信
3 返答(返信)

1,843件の閲覧回数
xkwy
Contributor I

Hi, igorpadykov

Thanks for reply.

I have already know that the chip's SPDIF are working well just as you provide dts&doc links.

my question is that I need another SPDIF for my application(the chip only have one), can it reachable by ESAI?

 

Best Regards!

 

0 件の賞賛
返信

1,835件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xkwy

 

> I need another SPDIF for my application(the chip only have one), can it reachable by ESAI?

 

not sorry.

 

Best regards
igor

 

0 件の賞賛
返信