ESAI I2S CONFIGURATION

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ESAI I2S CONFIGURATION

3,419 Views
abdulhussain
Contributor III

Hi,

I am trying to configure ESAI in normal mode with i2s data format for the configuration tx1 pin connected to external dsp. For this I have written dummy codec driver. But it is transmitting data only in tx0 pin. May i know how to drive data in tx1 pin instead of tx0. 

Regards,

Abdul

Tags (3)
4 Replies

3,124 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdul

one can try to change TEx bits in Transmit FIFO Configuration Register (TFCR),

simple example with ESAI configuration can be found in i.MX6 SDK (1.1.0_iMX6_Platform_SDK.zip) on

SMP Enable in IMX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,124 Views
abdulhussain
Contributor III

Hi Igor,

We are using imx8dx chipset. As you mentioned, sdk has bare metal programming example. We trying to achieve this configuration from Linux.

As per my understanding, fsl_esai_hw_params function in fsl_esai.c configures transmitter fifo enable bits based on the channels and slots,

u32 pins = DIV_ROUND_UP(channels, esai_priv->slots);

val = ESAI_xFCR_xWA(width) | ESAI_xFCR_xFWM(esai_priv->fifo_depth) |
(tx ? ESAI_xFCR_TE(pins) | ESAI_xFCR_TIEN : ESAI_xFCR_RE(pins));

Also in fsl_esai_trigger function, transmitter enable bits configured in TCR register which is also based on channels and slots.

So for example if i select channels as 2 and slots as 2 for normal mode, it gives pins value as 1 and select TX0 pins.

Can you guide us to drive data in normal mode from TX1 pin?

Regards,

Abdul

0 Kudos
Reply

3,124 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdul

I am afraid this is not configurable, so one will have to make

modifications in esai driver. Since these changes are not obvious and

straightforward due to complexity of alsa drivers, suggest to proceed with

extended support of NXP Professional Services | NXP 

Best regards
igor

0 Kudos
Reply

3,124 Views
abdulhussain
Contributor III

Thanks for the reply Igor.

0 Kudos
Reply