Solved! Go to Solution.
Hi mas
I doubt if one can get more high throughput than described on
i.MX6Q PCIe EP/RC Validation System, as solution was provided by nxp
engineering team based on internal design documentation.
>Please tell me how to calculate max throughput on PCIe RC of i.MX6.
there is no way to claculate it as throughput depends on many other
factors, like internal processor buses loading and delays in NIC-301 arbiters.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have an opposite question.
Since both PCIe and Display are sitting on the same Display switch of NIC-301 what to do to limit bandwidth on PCIe to avoid flickering on LVDS interface?
Do you have a sample code/example how to do it on i.MX6SoloX?
Do you have a corrected diagram for Chapter 43 of i.MX6SoloX reference manual rev.3 marked which ports are slave, which are masters which GPV_N belong to which peripherals, etc.
I'd also welcome information of what is the range of parameters in wr_tidemark, read_qos, write_qos.
Also, please tell me whether I should change values for AQoS CR Bandwidth and Sarutation and which Master corresponds to PER_S and Display switch on the diagram
Thanks,
--Alex
Hi Alex
such kind of support (with tweaking NIC-301) can be provided
with extended support of NXP Professional Services | NXP
Best regards
igor
Hi mas
I doubt if one can get more high throughput than described on
i.MX6Q PCIe EP/RC Validation System, as solution was provided by nxp
engineering team based on internal design documentation.
>Please tell me how to calculate max throughput on PCIe RC of i.MX6.
there is no way to claculate it as throughput depends on many other
factors, like internal processor buses loading and delays in NIC-301 arbiters.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
I understood I cannot get higher throughput than “i.MX6Q PCIe EP/RC Validation System” and cannot calculate max throughput. But I may be got max 211MB/s throughput based on measured values.
Thank you for your reply.
Best Regards,