ERRORs:while bitbake fsl-image-qt5 on Yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ERRORs:while bitbake fsl-image-qt5 on Yocto

2,575 次查看
1135279361
Contributor II

There are some errors occured while bitbake fsl-image-qt5 on Ubuntu-18.04,

Informations as follows, anyone have solution ?

-----------------/////////////////////////////////////////////------------------

WARNING: Host distribution "Ubuntu-18.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |#####################################################| ETA: 00:00:00
Loaded 2792 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-18.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qsabreauto"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "4.1.15-2.1.0"
TUNE_FEATURES = "arm armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:f5da2a5913319ad6ac2141438ba1aa17576326ab"
meta-oe
meta-multimedia = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-fsl-arm = "HEAD:be78894e4682f111575470fb23e51e6ba523508d"
meta-fsl-arm-extra = "HEAD:3dfb82fc7e703eae9891b3ffda0e9393701f2396"
meta-fsl-demos = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"
meta-bsp
meta-sdk = "HEAD:823b26a67261270d2bf22d511e6190641a8a90cf"
meta-browser = "HEAD:77736988073a5d90fcff9d0005c8477332ede387"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-qt5 = "HEAD:ccae79be69c5268df3b47e4e14cea0591c39a531"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks

-----------------/////////////////////////////////////////////------------------

ERROR: fsl-image-qt5-1.0-r0 do_rootfs: Error executing a python function in exec_python_func() autogenerated:

The stack trace of python calls that resulted in this exception/failure was:
File: 'exec_python_func() autogenerated', lineno: 2, function: <module>
0001:
*** 0002:license_create_manifest(d)
0003:
File: '/mnt/hdd/home/yezl/share/yocto/bin/fsl-release-bsp/sources/poky/meta/classes/license.bbclass', lineno: 48, function: license_create_manifest
0044: pkg_dic = {}
0045: for pkg in sorted(image_list_installed_packages(d)):
0046: pkg_info = os.path.join(d.getVar('PKGDATA_DIR', True),
0047: 'runtime-reverse', pkg)
*** 0048: pkg_name = os.path.basename(os.readlink(pkg_info))
0049:
0050: pkg_dic[pkg_name] = oe.packagedata.read_pkgdatafile(pkg_info)
0051: if not "LICENSE" in pkg_dic[pkg_name].keys():
0052: pkg_lic_name = "LICENSE_" + pkg_name
Exception: OSError: [Errno 2] No such file or directory: '/mnt/hdd/home/yezl/share/yocto/bin/fsl-release-bsp/build/tmp/sysroots/imx6qsabreauto/pkgdata/runtime-reverse/No'

ERROR: fsl-image-qt5-1.0-r0 do_rootfs: Function failed: license_create_manifest
ERROR: Logfile of failure stored in: /mnt/hdd/home/yezl/share/yocto/bin/fsl-release-bsp/build/tmp/work/imx6qsabreauto-poky-linux-gnueabi/fsl-image-qt5/1.0-r0/temp/log.do_rootfs.17984
$<50>ERROR: Task 9 (/mnt/hdd/home/yezl/share/yocto/bin/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-qt5.bb, do_rootfs) failed with exit code '1'
$<50>NOTE: Tasks Summary: Attempted 5832 tasks of which 5831 didn't need to be rerun and 1 failed.
No currently running tasks (4832 of 5838)

Summary: 1 task failed:
/mnt/hdd/home/yezl/share/yocto/bin/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-qt5.bb, do_rootfs
Summary: There were 73 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

标签 (3)
0 项奖励
回复
2 回复数

1,885 次查看
1135279361
Contributor II

I want to be able to build it on Ubuntu 18.04, and nothing else.

The same mistake, but the problem is not solved : https://community.nxp.com/thread/452080 

0 项奖励
回复

1,885 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ansel Yip,

Your safest bet is using Ubuntu 16.04, however, I understand that you wish to use Ubuntu 18.04. In that case I would recommend checking that all the required packages listed on the i.MX Yocto User’s Guide are installed in your system. (It could be that some packages are missing or not available in Ubuntu 18.04 and in this case you would need to manually install them if possible).

I hope this helps,

Regards,

0 项奖励
回复