i.MX6Q5E can't send DNS in android 5.1.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q5E can't send DNS in android 5.1.1

933件の閲覧回数
jimmyli
Contributor IV

Hi,

     In i.MX6Q5E platform, we run android 5.1.1 or android 6.0.1, and found that the DNS package couldn't be sent.

     Test process:

      1. DNS configuration :

          a. DNS with system setting;

          b. DNS with manual package;

     2. DNS package catching

         a. in system catching

         b. IP package catching outside

     3. Test result

         a. android 4.2.2   --OK, can catch the IP package outside

         b. android 5.1.1/6.0.1  --In system catching is OK, while IP package catching outside is not.

     Question:

     a. What cause the problem?

     b. How can we solve the problem?

     Thanks.

ラベル(2)
0 件の賞賛
返信
1 返信

849件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello Jimmy,

I apologize for the delay.

Do you know if there is a connection between your i.MX device and the modem that you are using?

The modem is recognizing the board?

Best Regards,

Diego

0 件の賞賛
返信