ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

2,644 Views
jiejia
Contributor III

board: refer to mx6q-sabresd

BSP: linux3.0.15

我在板子上面接了一个1080P的摄像头,按照Support BT1120 progressive mode in Mx6Q 提供的patch,给内核打上补丁。 

当我使用如下命令进行测试时,摄像头的图像是可以正常显示的:

./mxc_v4l2_overlay.out -iw 1920 -ih 1080 -it 0 -il 0 -ow 1280 -oh 800 -ot 0 -ol 0 -fr 30

但是当我使用自己写的一个v4l2程序来测试该摄像头时,执行到ioctl (v4l2_fd, VIDIOC_DQBUF, &tV4l2Buf),内核打印:ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0, 并且ioctl (v4l2_fd, VIDIOC_DQBUF, &tV4l2Buf)函数返回-1; 想请问下为什么会出现这种情况??

 

以下是测试程序的部分代码:

struct v4l2_format fmt;
struct v4l2_requestbuffers requestbuffers;
int v4l2_fd = -1;
int iError,i;

int type = V4L2_BUF_TYPE_VIDEO_CAPTURE;

v4l2_fd = open("/dev/video0", O_RDWR);
if (v4l2_fd < 0)
{
   printf(" open video ERR\n");
   return -1;
}

memset(&fmt, 0, sizeof(struct v4l2_format));
fmt.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
fmt.fmt.pix.pixelformat = V4L2_PIX_FMT_YUYV;
fmt.fmt.pix.width = 1920;
fmt.fmt.pix.height = 1080;
fmt.fmt.pix.field = V4L2_FIELD_ANY;
if((ioctl(v4l2_fd, VIDIOC_S_FMT, &fmt))<0)
{
   printf("Unable to set format: %d.\n", errno);
   return -1;
}

memset(&requestbuffers, 0, sizeof(struct v4l2_requestbuffers));
requestbuffers.count = 4;
requestbuffers.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
requestbuffers.memory = V4L2_MEMORY_MMAP;
if((ioctl(v4l2_fd, VIDIOC_REQBUFS, &requestbuffers))<0)
{
   printf("Error: failed to request buffers.\n");
   return -1;
}

buffers = calloc (4, sizeof (*buffers));
for (i = 0; i < 4; i++)
{
   memset(&tV4l2Buf, 0, sizeof(struct v4l2_buffer));
   tV4l2Buf.index = i;
   tV4l2Buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
   tV4l2Buf.memory = V4L2_MEMORY_MMAP;
   iError = ioctl(v4l2_fd, VIDIOC_QUERYBUF, &tV4l2Buf);
   if (iError)
   {
      printf("Unable to query buffer.\n");
      return -1;
  }
   buffers[i].start = mmap(0, tV4l2Buf.length, PROT_READ, MAP_SHARED, v4l2_fd,  tV4l2Buf.m.offset);
   if (buffers[i].start == MAP_FAILED)
   {
      printf("Unable to map buffer\n");
      return -1;
   }
}

for (i = 0; i < 4; ++i)
{
   tV4l2Buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
   tV4l2Buf.memory = V4L2_MEMORY_MMAP;
   tV4l2Buf.index = i;
   ioctl(v4l2_fd, VIDIOC_QBUF, &tV4l2Buf);
}

if((ioctl(v4l2_fd, VIDIOC_STREAMON, &type))<0)
{
   printf("error ioctl streamon\n");
   return -1;
}


fd_set fds;
FD_ZERO (&fds);
FD_SET (v4l2_fd, &fds);
select(v4l2_fd + 1, &fds, NULL, NULL, NULL);


tV4l2Buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
tV4l2Buf.memory = V4L2_MEMORY_MMAP;
iError = ioctl (v4l2_fd, VIDIOC_DQBUF, &tV4l2Buf); //在这里一直没有数据,然后内核打印超时,该函数返回-1
if (iError)
{
   printf("Unable to dqueue buffer. %d\n", iError);
   return -1;
}

 

Labels (2)
1 Reply

1,677 Views
joanxie
NXP TechSupport
NXP TechSupport

try to confirm if you have any I2C write issue, I2C write issue would cause this issue, and try to add delay and more print information for your code.